XAML Graphic Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Extensible Application Markup Language (XAML) Graphic object defines the attributes that represent a defined Graphics+ file for a given set of objects. XAML Graphic objects are created exclusively with the GGT and are saved on an ADS/ADX, ODS, SCT computer, or supervisory device as a file with an .xaml file extension.

Note: The Object Type for this object is labeled XAML Graphic in the software.

For detailed information on viewing XAML Graphic objects, refer to the Graphics+ Runtime Help (LIT-12011708).

For detailed information on the Graphic Generation Tool that is used to create and modify XAML Graphic objects, refer to the Graphic Generation Tool Help (LIT-12011697).

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.