Copying an Existing Graphic - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

Note: This is available when using the SCT only.

Procedure

  1. Click an existing graphic item in the Navigation Tree.
  2. On the Edit menu, select Copy.
  3. Click in the navigation tree where the new graphic is to appear.
  4. On the Edit menu, select Paste and name the new graphic.