Gauges: Dial Gauge Symbol - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

To bind Dial Gauge symbols to objects:

Procedure

  1. Double-click the Dial Gauge symbol. The Binding Information dialog box appears.
  2. Use the information in the following table to edit the fields.
    Table 1. Dial Gauge Symbol Options

    Field

    Description

    Object

    Allows you to type in the Item Reference of the object you want to bind to the Dial Gauge. Or, lets you click the Browse icon to launch a tree browser to select the object to bind to the Dial Gauge.

    Attribute

    Allows you to select the object’s attribute to bind to the gauge.

    Gauge Color

    Launches the color selector for the gauge to select the color displayed in the center of the gauge.

    High Limit

    Sets the high number for the display range of the gauge.

    Low Limit

    Sets the low number for the display range of the gauge.

    Units

    Displays the units used by the bound object.

    Status

    Displays the status of the bound object in the display box of the gauge.

    Properties

    Allows you to configure the text properties for the text in the display box of the gauge.

    OK

    Accepts changes.

    Cancel

    Cancels changes.