Value Display Boxes are useful for displaying the value and status of a large number of objects in a single graphic. The Value Display Box supports drag and drop functionality. If you select a single item or multiple items in the navigation tree and then drag and drop a Value Display Box, the box/es automatically binds to the selected item/s.
If a Value Display Box is configured to display the Status of the bound object, the text and box background appear in the standard Status Colors.
In View mode, Value Display Boxes appear as if they are editable boxes, but they are not. Double click on the Value Display Box to display the Focus view for the bound object and right click to show the command menu.
See the Value Display Boxes step section for information on binding Value Display Boxes.