Format - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Format menu choice contains the choices listed in the following table.

Table 1. Format Menu Options

Choice

Description

Copy Binding

Copies the selected symbol’s binding information, which you can then paste to a new symbol. With this feature, you can easily bind several symbols to one object.

Paste Binding

Pastes the previously copied binding information to the selected symbol(s).

Copy Format

Copies the selected symbol’s formatting (size and font information), which you can then paste onto another symbol. This allows you to easily format multiple symbols in the same way.

Paste Format

Pastes the previously copied formatting information to the selected symbol(s).