Align - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Align menu choice contains the choices listed in the following table.

Table 1. Align Menu Options

Choice

Description

Note: When you select multiple objects by dragging the mouse across them, the first selected symbol is not based on the symbol's location within the graphic, but on the order in which it was originally added to the graphic. We recommend that you first click on the symbol with which you want to align other symbols. Once you have selected that symbol, hold down the Shift key while you drag the mouse across additional symbols to select them (you can also use Shift + click to select additional symbols).

Align Top

Aligns all symbols to the top most edge of the first symbol you selected.

Align Bottom

Aligns all symbols to the bottom most edge of the first symbol you selected.

Align Left

Aligns all symbols to the left most edge of the first symbol you selected.

Align Right

Aligns all symbols to the right most edge of the first symbol you selected.

Align Horizontal Center

Aligns all symbols to the horizontal center of the first symbol you selected.

Align Vertical Center

Aligns all symbols to the vertical center of the first symbol you selected.