Opening the Trend Module - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

To open the Trend Module for an object on a Graphics+ graphic, click View Trend from the element’s User Actions Panel. The Trend Module appears with the charted trend data. If more than one trended attribute is available, click View Trend to display a submenu that lists all available trended attributes. Click a trended attribute to open the Trend Module.

Figure 1. Selecting a Trend to Add to the Trend Module

If you want to open the Trend Module without adding or changing its content, click the Tools drop-down arrow on the Graphics+ Display Control tool and select Trend. The Trend Module reappears in its last state and condition.

Figure 2. Reopening the Trend Module