Commands - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

You can command objects that are bound to graphic symbols using two methods. The first method is to left-click the object’s Inline Command Box or Advanced Value Box, then edit the value of the object. If commanding is disabled for that symbol, the value is not be editable. The second method is to right-click the object’s Inline Command Box, Advanced Value Box, or other elements of Graphics+ symbols such as gauges, to open the User Actions Panel, then select More Commands to bring up the Metasys commands dialog box. With both methods, if you are not authorized to command the object, the command selection is disabled.