Graphic Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Graphics object defines the attributes that represent a defined user graphic for a given set of objects. Graphic objects must exist under a container object or under another Graphic object (this allows you to link graphics together).

For detailed information on the User Graphics Tool, refer to the User Graphics Tool section in the Metasys SMP Help (LIT-1201793).