Enable - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Enable command allows the Schedule object to resume normal scheduling operation. The Schedule object starts the schedule as soon as it is enabled. When it is re-enabled, the Schedule object writes its current value to the scheduled items.