The Schedule object works behind the scenes of the Scheduling feature. The Schedule object updates attribute values of objects according to the time of day. These times can be specified for days of the week and as exceptions.
When you create a Schedule object at a BACnet client and map the object to a network engine, a folder called Schedule is created and a new Schedule object is created under that folder in the navigation tree.
For more information on the Scheduling feature or the steps it takes to create one, refer the Scheduling section in the Metasys SMP Help (LIT-1201793).