Multistate Output Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Multistate Output object’s attributes represent the desired state of one or more physical outputs or processes of the device in which the object resides. The actual functions associated with a particular state are determined locally (not part of protocol). Present Value represents the state with a number, and State Text associates a description with each state.

The Multistate Output object integrates N1, N2, and BACnet controllers with supervisory controllers, resulting in:

  • a consistent interface to point objects for all controller types

  • flexibility in point mapping

  • support for Metasys controllers

For example, this object allows you to command the modes of an access control device from a supervisory controller.

Note: The N1 migration Multiple Command object maps to this Multistate Output object.

For general information on Metasys system objects, see Common Object Attributes.