Event Enrollment Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Menu Selection: Insert > Object > Event Enrollment

The Event Enrollment object’s attributes represent and contain information for managing events. Events are changes in the value or state of an object that meet specific criteria. The Event Enrollment object defines the event criteria and provides a connection between an event and a notification message sent to recipients. A recipient device is enrolled for notification if:

  • it is one of the recipients in a Notification Class Object referenced by the Event Enrollment object

  • a Notification Class object is not referenced and it is the recipient of the Event Enrollment object

When you create an Event Enrollment object at a network engine using a BACnet client, a new Event Enrollment object is created under that folder in the navigation tree.