Channel Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Menu Selection: Insert > Object > Channel

The Channel object allows a third-party BACnet workstation to represent a Channel object in a BACnet field controller. The Channel object allows for the efficient adjustment of lighting brightness values to multiple lighting controllers. For example, with the Channel object, you can create logic in a BACnet field controller to turn lights on based on the state of occupancy sensors provided by the BACnet-based lighting system.