Analog Value Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Insert > Object > AV

Analog Value (AV) objects have similar software characteristics and capabilities to Analog Input Objects; however, Analog Value objects are not associated with any physical hardware and are the result of a control process or operator entry. This object allows you to hold an analog value for other objects to reference. For example, an LON Integration Object can reference and base its operation on an analog value such as Outdoor Air Temperature Low Limit.

For general information on Metasys objects, see Common Object Attributes.