This object contains attributes common to many Metasys system objects.
| Name / View Group Attribute ID Writable (W) Configurable (C) |
Attribute Description |
|---|---|
| Min Value -- Engineering Values 69 W C |
Defines the lowest reliable value (in engineering units) for the Present Value. |
| Max Values -- Engineering Values 65 W C |
Defines the highest reliable value (in engineering units) for the Present Value. |
| Relinquish Default -- Engineering Values 104 W C |
Specifies the default value to be used for the Present Value attribute when no commands are currently controlling this object. If this attribute is configured to any value other than None, the object sends commands for the value immediately. |
| Units -- Display 117 W |
Indicates the engineering measurements units used by the object. |
| COV Increment -- Display 22 W |
Specifies the minimum change in Present Value required for the object to report a change. |
| Display Precision -- Display 661 W C |
Defines the decimal rounding and the decimal places to display of the Present Value and associated attributes. |
| Use Remote Alarming -- BACnet 853 W C |
When the attribute Intrinsic Alarming Defined is set to True, determines where alarms for the object originate. If the remote integrated object contains attributes for originating alarms, then Use Remote Alarming defaults to True, causing the local mapper object to accept alarms from the remote integrated object that are routed to the NxE. If the remote integrated object does not contain attributes for originating alarms, then Use Remote Alarming defaults to False causing the local mapper object to originate alarms. When Use Remote Alarming is false, any alarms from the remote integrated object are ignored at the NxE. If the value of Use Remote Alarming is changed, a restart of the NxE may be required to assure correct operation. This attribute applies only to BACnet integrations. |
| Intrinsic Alarming Defined -- BACnet 569 W C |
Enables the BACnet Intrinsic Alarming feature in the object and the definition of related attributes. For detailed information, see BACnet Intrinsic Alarming. For more information, refer to the BACnet Intrinsic Alarming section of the Metasys SMP Help (LIT-1201793). |
| Device Type -- BACnet 31 W C |
Contains a description of the physical device connected to the object |