Analog Output Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The AO object’s attributes represent the external, visible characteristics of an analog output. This object integrates N1, N2, and BACnet controllers into supervisory controllers, resulting in:

  • a consistent interface to point objects for all controller types, so they appear as a homogenous set to the user interface

  • flexibility in point mapping

  • permanent update of setpoints in controllers. The user has the ability to write to the permanent memory of some controllers.

  • support for all Metasys controllers

  • For example, this object allows you to command a damper to a given position from a supervisory controller.

For general information on Metasys system objects, see Common Object Attributes.