Analog Input Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

This object contains attributes common to many Metasys system objects.

Table 1. Analog Input Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description
Display Precision -- Display

661 W C

Defines the decimal rounding and the decimal places to display for the Present Value and associated attributes.
Units -- Display

117 C W

Indicates the engineering measurement units used by the object.
COV Increments -- Display

22 W C

Defines the minimum change in the Present Value required for the object to report a change.
Intrinsic Alarming Defined -- BACnet

569 W C

Enables the BACnet Intrinsic Alarming feature in the object and the definition of related attributes. For detailed information, see BACnet Intrinsic Alarming.

Use Remote Alarming -- BACnet

853 W C

When the attribute Intrinsic Alarming Defined is set to True, determines where alarms for the object originate. If the remote integrated object contains attributes for originating alarms, then Use Remote Alarming defaults to True, causing the local mapper object to accept alarms from the remote integrated object that are routed to the NxE. If the remote integrated object does not contain attributes for originating alarms, then Use Remote Alarming defaults to False causing the local mapper object to originate alarms. When Use Remote Alarming is false, any alarms from the remote integrated object are ignored at the NxE. If the value of Use Remote Alarming is changed, a restart of the NxE may be required to assure correct operation. This attribute applies only to BACnet integrations.

Device Type -- BACnet

31 W C

Contains a description of the physical device connected to the object.
Min Value -- Engineering Values

69 W C

Defines the lowest reliable value (in engineering units) for the Present Value.
Max Value -- Engineering Values

65 W C

Defines the highest reliable value (in engineering units) for the Present Value.