Wireless Sensor Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

There is a Wireless Sensor object in the field point object for each wireless temperature sensor mapped to the NAE. The Wireless Sensor object receives communications from the wireless sensor.

All integrated wireless field points (Wireless Sensor objects) appear under the Wireless Receiver Objects (field devices), which appear under the Wireless Receiver Supervisor Object in the Navigation Tree.

Note: The Wireless Sensor object is not available for network engines updated to Release 9.0.7 or later.