VND Controller Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.

Table 1. VND Controller Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description

Enabled -- Object

673 W C

If True, allows communication to the vendor device. If False, prevents communication to the vendor device.

Enabled -- Status

673 W C

If True, allows communication to the vendor device. If False, prevents communication to the vendor device.

Offline -- Status

913

Displays the offline or online status of connected hardware.

Graphic Alias -- Graphic Association

32623 W C

Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this vendor device.

Graphic -- Graphic Association

32581 W C

Indicates the graphic associated with the vendor device.