NCM Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.

Table 1. NCM Object Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description

NCM Name -- Engineering Values

2562 C

Represents the defined name of the NCM as it appears in the existing N1 network.

Poll Delay -- Engineering Values

1163 W C

Displays the polling time for non-triggerable attributes in milliseconds. The poll delay is the time between NIE polls to the N1 network points.

Disable Automatic Alarming -- Engineering Values

1396 W C

Specifies whether automatic online/offline device event reporting is disabled (True) or enabled (False). This attribute only applies to the device and not to the device’s mapped objects. Devices with the Disable Automatic Alarming attribute set to True suppress the alarm event but still indicate they are offline in the navigation tree with a red X. Alarm extensions are not affected by this attribute.

Graphic -- Graphic Association

32581 W C

Indicates the graphic associated with the NCM.

Graphic Alias -- Graphic Association

32623 W C

Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this NCM.