Create NCM objects by adding NCMs to the system Navigation Tree. The attributes of the NCM object are read from the NCM device. The NCM object attributes update periodically based on the poll delay attribute of the parent N1 Migration Object. The NCM object can only be a child object to the N1 Migration object. Add more NCM objects with the Field Device.
For general information on Metasys system objects, see Common Object Attributes.