IP Field Controller Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The IP Field Controller object defines a standardized BACnet object with attributes that represent the external, visible characteristics of a device. Only one Device object exists in each IP Field Controller. The IP Field Controller object appears as a child of a BACnet Integration object.