BACnet Device Object Commands - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The following table lists the commands supported by the BACnet Device Object.

Table 1. BACnet Device Object Commands
Command Name Parameters Description

Rediscover Text Strings

None

Resets the States Text across a supervisory device by rediscovering text strings from all mapped BACnet objects.

Note: When the Rediscover Text Strings command is sent from the Site Director device UI to another supervisory device and the UI is running on the supervisory device, you must close and restart the UI on the supervisory device in order for the text to appear correctly.
Reset Field Device

Type: Cold Start or Warmstart

Password

Resets the BACnet device.

Sync Field Device Times

None

Sends a high-priority time synchronization command to child devices, based on the device mapper object's Manual Time Sync Type.