BACnet Device Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The BACnet Device object defines a standardized BACnet object with attributes that represent the external, visible characteristics of a device. Only one device object exists in each BACnet Device.

Notes:
  • The Johnson Controls network engine device object includes attributes and methods not required by the BACnet Device object. For information on the network engine device object, see the Engine Device Object section.
  • The Object Type for this object is labeled Non-FEC BACnet Device in the software.