Printing the Entire Help System - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

The entire Help system is available for printing in Adobe PDF format.

To print the entire Help system:

Procedure

  1. If necessary, download Adobe ReaderĀ® (required to view the PDF file) from the Adobe Reader site.
  2. Go to the QuickLIT Product Information website.
  3. In the tree on the left, browse to Metasys System > General System Information .
  4. On the right side of the window, click Metasys System Help (PDF format). The Help PDF opens in Adobe Reader.
  5. On the File menu of Adobe Reader, select Print.

Results

Note: This file is large (approximately 800 pages). Allow adequate time for downloading and printing.