Help Menu - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Metasys Help files provide shared system information and individualized, mode-dependent information for the Metasys Site Management Portal (SMP) or the System Configuration Tool (SCT). The Metasys SMP Help (LIT-1201973) and Open Data Server Help (LIT-12011942) provide information about alarming, commanding, auditing live data values, and other online features. The Metasys SCT Help (LIT-12011964) provides information about offline operations such as managing archives, creating spaces, simulating systems, and establishing equipment and serving relationships.

In either SMP or SCT mode, the Metasys System Help menus provide Help files in PDF format. Refer to the QuickLIT website for the most up-to-date version of the Metasys Help files.

For more information on the modes of operation, see Modes. For a description of the Authorized Required column, see Authorized Menu Items.