Updating point settings - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Beginning at SCT Release 14.0 a semantic data point model is supported with a Metasys 11.0, or later, site director. Using SCT 14.0 with Metasys 10.1 does not support this feature. Data point modelling facilitates sharing data and its meaning across applications and business processes through simplified aggregation.

Use the Update Point Settings feature to update the following points in an archive:

  • Internal ID - Do not modify
  • Display Name - Do not modify
  • Description - Do not modify
  • Factory Shortnames - Do not modify
  • Custom Shortnames

You can export point data to a file, edit the file in a spreadsheet application such as Microsoft Excel, and then import the file to update the archive.