Updating Object Labels - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Use the Update Object Labels feature to update the display name and description attributes of the following objects in an archive:

  • Equipment
  • Spaces
  • Controllers
  • Controller templates
  • Equipment definitions

You can export each category of objects to a file, edit the file in a spreadsheet application such as Microsoft Excel, and then import the file to update the archive. If you update an object's display name attribute, its FQR is not altered, and no references or object relationships are changed.