Configuring the Metasys UI with SCT overviews - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29
Figure 1. Configuring New Sites with the Metasys UI

Figure 2. Configuring Existing Sites with the Metasys UI

Note: From Metasys UI Release 2.1, you can associate all graphic types in the Graphics Manager of JCT and Metasys UI. Refer to the Johnson Controls System Configuration Tool (JCT) Help (LIT-12012116) for more information.

For more information about room schedules, controller templates, and the Rapid Archive Field Controller wizard, see the Rapid Archive Creation section. For more information about associating graphics, see the Graphics Association section.