Exporting Device Information from SCT - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Procedure

  1. From the Facility menu, click Rapid Archive.
  2. In the Select Scope window, select the Supervisory Devices to export information from, then click Open. The Rapid Archive Field Controller Wizard appears.
  3. Click Export.
  4. Navigate to the location where you want to save the file, enter a file name, then click Export. The file is saved with a .csv extension.
  5. If the export is successful, a confirmation message appears. Click OK.