Rapid Archive Schedule Population in the Rapid Archive Wizard - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

To streamline archive configuration, use the Rapid Archive wizard to generate archives based on .xls Rapid Archive Schedule files. You import the Rapid Archive Schedule files into the Rapid Archive Field Controller wizard.

Important: Use version 3 of the Rapid Archive Schedule with SCT Release 13.0 and later. At Release 13.0 the Rapid Archive Schedule spreadsheet is installed on the SCT computer at C:\Users\Public\Public Documents\RAC.

If you are a Johnson Controls employee, you can view informational videos about Rapid Archive Creation (RAC) on the uLearn site: https://jc.kzoplatform.com/containers/928995312607959016.

Figure 1. Sample Rapid Archive Schedule

Keep in mind the following recommendations when working with Rapid Archive Schedules:

Important: The Rapid Archive Field Controller wizard is case-sensitive.
  • You must not edit Column headings in the Rapid Archive Schedule file that are used by the Rapid Archive Field Controller Creation wizard feature. At SCT Release 13.0 you can reorder the columns and insert custom columns for your own reference, and not affect the import.
  • You can alter columns not specifically called out in the following table and not impact the Rapid Archive Field Controller Creation wizard process.
  • You can pre-select the supervisory devices that you want to edit in the all Items tree, prior to opening the rapid archive feature. If you do not pre-select any supervisory devices, the Select Scope window appears after launching the rapid archive feature.
  • As best practice, create multiple Rapid Archive Schedules based on device-level hierarchy, for example, individual room schedules for chillers, boilers, air handling units, and terminal units.
  • If you are required to enter a name, use the Name attribute of the Object.
Table 1. Rapid Archive Schedule Requirements and Descriptions

Rapid Archive Schedule Column Heading

Used by RAC

Requirements and Description

Space Information

Site/Building/Floor

Yes

Enter the full Spaces location for the device to be added to ensure proper Spaces tree auto-creation. For example, BE Headquarters/Campus 507/Building 9/Floor 2 creates the four space parent space hierarchy levels BE Headquarters, Campus 507, Building 9, and Floor 2.

This column populates the Spaces tree information in SCT.

Room Number

Reference Only The Room Number is provided as a local reference column and does not populate the Space tree in SCT.

Leaf Space (e.g. Room)

Yes

Not required if the equipment serves the whole campus.

Enter the Leaf Space for the Site > Building > Floor hierarchy that is associated to the Equipment being created.

All Items / Equipment Tree Information

Device Name

Yes

Enter the Controller Name as you want it to be displayed in the All Items tree and Equipment tree.

This column populates the Name column in the Rapid Archive wizard.

Device FQR Reference

Yes

Enter the Controller's FQR as you want it to appear in the SCT UI and tool tips.

We recommend that you copy the Controller Name as written in the Device Name column over to the Device FQR Reference column.

The key purpose of a different FQR name is for existing sites that had standard naming processes established for the FQRs in SMP and SCT.

Device Description Yes (optional)

Enter an optional description. This column populates the Description column in the Rapid Archive wizard.

Equipment Name Yes

Enter the Controller Name as you want it to be displayed in the Metasys UI's Equipment views.

Served By Equipment Name

Yes (optional)

Enter the exact name of the pre-existing device serving your controller.

This column populates the Served By relationship in the Rapid Archive wizard.

Note: The device serving your controller must already be created in the SCT archive, or the serving relationship is not created through the Rapid Archive wizard.

Controller Part #

Reference Only

The Controller Part # column is provided as a local reference column that does not populate any columns in the Rapid Archive wizard but can be used to display whether the device is JCI family or Generic family.

Network Information

Engine Name

Yes

Enter the name of the parent NAE exactly as it appears in SCT.

This column populates the Supervisory Device column in the Rapid Archive wizard.

Note: The parent NAE to your controller must already be created in the SCT archive, or the relationship is not created through the Rapid Archive wizard.

Trunk Name

Yes

Enter the Trunk Identifier for the integration trunk for your device. Integration trunk IDs are populated based on their port assignments on the physical field devices.

This column populates the Integration column in the Rapid Archive wizard.

Notes:
  • The trunk for your controller must already be created in the SCT archive, or the integration relationship is not created through the Rapid Archive wizard.
  • For MSTP Trunks, remember to set the Trunk Number in the Hardware Tab of the MSTP Integration when the trunk is created. This is required to support both the hardware and remote field buses.
    • MSTP trunks also have their own MAC Address column that must be filled in.
  • For IP Trunks, you can only create and name one IP integration per engine.
    • IP trunks also have their own IP Controller Number column that you must fill in.

Controller Host Name (Future)

Reference Only The Controller Host Name column is provided as a local reference column that does not populate any columns in the Rapid Archive wizard but can be used to display the network host name of the device.

JCI MAC Address

Yes

Enter the MAC address for the device. The uniqueness of the MAC Addresses per MSTP integration is be validated in Rapid Archive after you import.

This column populates the JCI Mac Address column in the Rapid Archive wizard.

Note: For MS/TP Trunk, a unique MAC Address per engine per MSTP Trunk is required. The MAC Address is 8 position dip switch setting on the MSTP controllers or 3 digit rotary dial for CxM controllers.
Note: For third party MS/TP devices this column should remain empty.
IP Controller Number Yes

Enter the combined value of rotary switches set on the device. The uniqueness of the Controller Numbers is be validated by the Rapid Archive wizard after you import.

This column populates the IP Controller Number column in the Rapid Archive wizard.

ZigBee PANs Offset

Reference Only

The ZigBee PANS Offset column is provided as a local reference column for users configuring a WNC mesh and does not populate any columns in the Rapid Archive wizard.

Instance # (BACoid)

Yes

Enter a unique device identifier number based on the entire site. The uniqueness of the Instance # (BACoid) is be validated by the Rapid Archive wizard after you import.

If you leave this cell blank, SCT assigns the device the next available instance number.

This column populates the Instance Number column in the Rapid Archive wizard.

Note: This value is required for third party devices.
N2 Address Yes  

DHCP Enabled

Yes

Enter True or False to enable or disable DHCP for each controller.

IP Address

Yes Enter the IP Address for the device.

This column populates the IP Address Column in the Rapid Archive wizard

Subnet Mask

Yes (optional) Enter the Subnet mask used for the IP address.

This column populates the IP Mask column in the Rapid Archive wizard.

IP Router Yes (optional) Enter the Router's IP address for the device.

This column populates the Router IP Address Column in the Rapid Archive wizard

ETH-1 Reference Only

The ETH-1 column is provided as a local reference column for the controller's input and does not populate any columns in the Rapid Archive wizard.

ETH-2 Reference Only

The ETH-2 column is provided as a local reference column for the controller's output and does not populate any columns in the Rapid Archive wizard.

Definitions and Templates

Equipment Definition Name

Reference Only

The Equipment Definition Name column is provided as local reference column and does not populate the Equipment or All Items tree.

Note: Only Equipment Definitions linked to Controller Templates in your SCT archive prior to importing the Rapid Archive Schedule are used to populate the Equipment Tree.

We recommend one equipment definition be used to create many Equipment Instances of the same type. For example, one Single Duct VAV definition could be created for all Single Duct VAV Boxes that are cooling only, cooling with reheat, or fan powered.

Controller Template Name

Yes Enter the controller template name as displayed in the SCT UI.
Note: The controller templates must exist in SCT prior to importing the Rapid Archive Schedule for proper linking.

This column populates the Controller Template column in the Rapid Archive wizard.

Parameters

SA-AREA

No Enter the Supply Area value to write to the controller's CAF.

SA-KFACTOR

No Enter the default K Factor value to write to the controller's CAF.

CLG-MAXFLOW

No Enter the Cooling Max Flow value to write to the controller's CAF.

CLGOCC-MINFLOW

No Enter the occupied cooling minimum flow setpoint value to writer to the controller's CAF.

HTGOCC-MINFLOW

No Enter the occupied heating minimum flow setpoint value to write to the controller's CAF.

<CUSTOM CAF PARAMETERS>

No Enter additional parameters manually following the Rapid Archive Schedule's format for customized parameters.

To view all available attributes for custom parameters view the CAF Parameter Sheet.