Creating a Controller Template Based on Existing Controllers - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29
Note: This procedure populates points for a new template. For existing templates that have points, the point list is deleted and repopulated based on the existing controller.
  1. Select a controller template from the All Items tree. If you do not have a pre-existing controller template, create a new template through the Insert > Object > Object Type > Controller Template wizard.
  2. Open the controller template with a double-click or right-click and select View.
  3. Select the Point List tab and click Get Points. The Select Field Controller window appears.
  4. Select the field controller you want to copy a point list from and click OK. The Get Points dialog box appears.
  5. Click Create point list. The point list is repopulated from the selected field controller.