Assigning Controller Templates with the Rapid Archive Field Controller wizard - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

Users can assign controller templates to controllers using the Rapid Archive Field Controller wizard.

Procedure

  1. Open the Rapid Archive Field Controller wizard.
  2. Click Edit, then navigate to the controller you want to assign a template to.
  3. In the Controller Template column, click the drop-down arrow. The drop-down menu appears.
  4. Select the template you want to assign the controller.
  5. Repeat steps 3 and 4 for all controllers you want to assign controller templates to.
    Note: If a controller has an existing template assigned, an asterisk will appear to the left of the template name (Figure 1). Leave the current controller template selection in place to maintain the current point structure for the controller. To modify the template, see Modifying Controller Templates with the Rapid Archive Field Controller wizard.
    Figure 1. Existing Controller Template Selection
  6. Click Save.