An Equipment Definition object can only be created through the option.
|
Attribute Name |
Data Type |
Initial Value |
Values/Options/Ranges |
|---|---|---|---|
|
Name |
Text |
Blank |
Maximum length of 400 characters |
|
Description |
Text |
Blank |
Maximum length of 64 characters |
|
Authorization Category |
One type from a set |
HVAC |
HVAC, Fire, Security, Services, Administrative, General, Lighting, Refrigeration, Critical Environment, Air Quality, Power, Energy, System Custom 1–150 |
|
System Subtype Set |
One type from a set |
Subsystem Category |
Various |
|
System Subtype |
One type from a set |
Terminal Units |
Terminal Units, Air Handlers, Central Plants, other types |
|
Graphic |
Graphic Object |
Blank |
Various |
|
Column |
Description |
|---|---|
|
Display Data |
Select the check box to select a row for display data point in the Metasys UI. |
|
Label |
Contains the description of the point (for example, Zone Setpoint). |
|
Short Name |
Contains an abbreviated name of the point (for example, Flow Percent). Note: Do not leave the Short Name field blank.
|
| Type | Displays the semantic data point model name mapped to short name by the Point Setting dataset. See Updating point settings. |
|
Instance |
Displays the Instance Number of the object on the remote field device. The Instance number, along with the object type, defines the remote object’s BACnet Object Identifier. The BACnet Object Identifier is used to establish communication with the object. Note: Points are matched by their instance number before matching on the
Search Column criteria.
Important: If you create an Equipment Definition for a
third-party device, and there are duplicate instance numbers, you must use the
Search Criteria column. Only use the
Instance column if the instance number
for a network point on a controller is unique.
|
|
Net Point Address |
Contains the Metasys N2 Point Address associated with a point. This is a comma-delimited list of instance number. |
|
Net Point Type |
Contains the Metasys N2 Point Type associated with the point. |
|
Search Criteria |
Contains user-defined search criteria for points. Search
criteria can contain the following:
|
| Category | Displays the category number of the point. |