Associating a Standard Graphic to a Space Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Standard graphics configured for the site.

Any graphics associations performed in SCT require a download to the ADS/ADX to view the graphics in the Metasys UI. A download is not required to view the graphics in the JCT.

To associate a Standard graphic to a Space object in SCT:

Procedure

  1. Select the Space object in the Spaces tree.
  2. In the Configuration tab of the Space object, click Edit.
  3. Select the Standard graphic from the All Items tree. Drag the Standard graphic to the Graphic attribute field.
    Note: You can have several graphics associated to a Space object.
  4. Click Save.