Associating a Standard Graphic to a Field Controller - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Standard graphics configured for the site.

Any graphics associations performed in SCT require a download to the ADS/ADX (and the engine, if changes were made to the engine) to view the graphics in the Metasys UI. A download is not required to view the graphics in the JCT.

To associate a Standard graphic to field controller in SCT:

Procedure

  1. Select the field controller from the All Items tree.
  2. In the Configuration tab of the field controller, click Edit.
  3. Select the standard graphic from the All Items tree. Drag the standard graphic to the Graphic attribute field.
    Notes:
    • Only one Standard graphic or Graphics+ graphic can be associated to a field controller.
    • If a graphic is associated to a field controller, you do not need to associate the graphics to equipment that was derived from the controller.
  4. Click Save.