Associating a Graphics+ Graphic to a Field Controller - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Graphics+ graphics configured for the site.

Any graphics associations performed in SCT require a download to the ADS/ADX (and the engine, if changes were made to the engine) to view the graphics in the Metasys UI. A download is not required to view the graphics in the JCT.

To associate a Graphics+ graphic to field controller in SCT:

Procedure

  1. Select the field controller from the All Items tree.
  2. In the Configuration tab of the field controller, click Edit.
  3. Select the Graphics+ graphic from the All Items tree. Drag the Graphics+ graphic to the Graphic attribute field.
    Note: You can have several graphics associated to a field controller.
  4. Click Save.