Associating Graphics+ Graphics to a Space Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

The following steps presume that you are logged into SCT and your archive has spaces, equipment, Equipment Definitions, and Graphics+ graphics configured for the site.

Any graphics associations performed in SCT require a download to the ADS/ADX to view the graphics in the Metasys UI. A download is not required to view the graphics in the JCT .

To associate a Graphics+ graphic to a Space object in SCT:

Procedure

  1. Select the Space object in the Spaces tree.
  2. In the Configuration tab of the Space object, click Edit.
  3. Select the Graphics+ graphic from the All Items tree. Drag the Graphics+ graphic to the Graphic attribute field.
    Note: You can have several graphics associated to a Space object.
  4. Click Save.