Exporting Spaces - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

Exporting a space or spaces lets you share or quickly create spaces.

Procedure

  1. Go to Item > Export Item.
  2. In the Export Archive wizard, select a space from the Spaces Tree tab.
    Note: You can export any space available. However, to import the space into an archive, the ADS/ADX structure must be the same between the source archive and the destination archive. The ADS/ADX name and version must be the same as well.
  3. Follow the wizard screens. Click Finish.