Find and Replace to Assist Auto-Discovery Serving Relationships - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

If serving relationship fields do not auto-discover:

Procedure

  1. Right-click the Equipment Name or Equipment Description column heading. Click Find and Replace.
    Note: To make single edits, select the individual equipment, right-click the Equipment Name or Equipment Description column headings, and click Find and Replace (in selection).
  2. The Find and Replace window appears. Enter the criteria for the Find field and the Replace field. To replace all matching text, select Matching Text. To replace all non-matching text, select Non-Matching Text.
    Table 1. Find and Replace Search Criteria

    Character

    Search Description and Application

    An asterisk (*)

    Use before and after the search criteria text to search that portion of the text. For example, *ZN-T*.

    Use in the search criteria text lets you search for zero or more of any character. For example, Z*-T returns results including ZN-T and ZONE-T.

    A question mark (?)

    Use in the search criteria text to search for zero or one instance of any character. For example, Hum?-C returns results including Hum1-C and Hum-C.

    A percent symbol (%)

    Use in the search criteria text to search for numerals 0 through 9. For example, Hum%-C returns results including Hum1-C and Hum7-C. You can enter multiple % to search for text that contains multiple numerals. For example, Hum%%-C returns results including Hum26-C. This also matches the percent symbol itself, such as in: % Humidity.

    A pound sign (#)

    Use in the search criteria text to search for a string of one or more numerals. For example, #BoxHtg-C returns results including 1BoxHtg-C and 34BoxHtg-C. This search also matches the pound sign itself, such as in: BLDG #1.

    Normal Text

    Use in the search criteria to return results that match the characters exactly without matching case. For example, zn-t returns results for ZN-T and zn-t.

  3. Click Replace All.
  4. Right-click the Serving column heading. Click Rediscover Spaces.
  5. Repeat Steps 1 through 4 for each equipment that you wish to create serving relationships.