Defining Equipment or Space Serving Relationships - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

Note: If you are using Global Modify to edit serving relationships, understand that this function replaces all serving relationships for the selected spaces or equipment. To add or minimally edit serving or Served By relationships for spaces or equipment without replacing all relationships, use the following procedure:

Procedure

  1. Go to the All Items tree.
  2. Right-click the Equipment Definition for the equipment that needs a serving relationship.
    Figure 1. Equipment Definition Action Menu

  3. Select Open in Discovery. The Equipment Discovery window opens.
  4. Go to the Spaces or Equipment Tree.
  5. Select all spaces or equipment that need Served By relationships.
  6. Drag the selected spaces to the Serving column of the Equipment Discovery window.
    Figure 2. Drag Spaces to Serving Column

  7. Click Save.