Auto-Discovery Guidelines and Workflow - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English
guidelines:
  • Spaces must be created for auto-discovery to properly function; however, Served By relationships do not need to be pre-defined.
  • Field Controllers' name or description fields must contain the name of their associated Space name.
  • NAE description fields must contain the parent-space name. For example, the name must include the building name or room names.
  • Equipment Definition objects must have display points set up and checked out.

Follow these steps to use the NAE Drag and Drop feature of the Auto-Discovery Serving Relationship.

  1. On the Facility Menu, select Discover Equipment to complete the auto-discovery of equipment and serving relationships.
  2. Drag the NAEs into the Equipment Discovery window. Controllers with mapped points appear in the table.
  3. Check the list of controllers and remove any additional selections.
  4. Right-click the Serving column heading and select Rediscover Spaces. Spaces that match the NAE and controller description fields are auto-discovered and populated in the table.
  5. Verify the Serving relationships, and if needed, add any additional space association manually.
  6. Save the Equipment Discovery window.