Runtime Totalization - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Runtime Totalization extension tracks the time that elapses while a designated input, such as a binary or multistate value, matches a specified state.

These two essential parameters determine the Runtime Totalization extension’s mode of operation:

  • the monitored Input Reference

  • the Reference (state) that identifies active runtime

Use this extension to track the amount of time that a piece of equipment, such as a fan or a pump, is operational. This extension also determines the amount of time that a point is in alarm or the runtime of fixed loads (such as lighting) for energy consumption and tenant billing.

For detailed information on the Runtime Totalization extension, see Runtime Totalization Attributes.