Event Totalization Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Event Totalization extension contains attributes common to Metasys system objects. For details, see Common Object Attributes.

The following table lists the attributes specific to the Event Totalization extension. Click the attribute name in the table for a description of the attribute. Letters in the Notes column indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.

Table 1. Event Totalization Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Display Precision

C,W

1s

Uses Display Precision (Set 0).

Executing

 

Active

Active

Totalize Limit

Inactive

Active: The extension is calculating and has not reached the Totalize Limit.

Totalize Limit: The extension has reached the limit and has stopped calculating because Rollover is set to False.

Inactive: The extension is unreliable or disabled and is not calculating.

Input Reference

C

   

Present Value

C,D,R,W

   

Reference

C,W

State 0

States Text attribute identifies the enumeration set for this attribute.

Reliability

 

Reliable

Uses Reliability (Set 503).

Reset

(This attribute does not appear in a view, but may be scheduled and trended.)

W

False

False

True

Reset Date

     

Reset Time

     

Rollover

C,W

False

False

True

Rollover Count

R,W

0

0–4,294,967,295

Scale Factor

C,W

1.0

Minimum Value > 0

States Text

(This attribute does not appear in a view, but may be scheduled and trended.)

C,W

States

 

Totalize Limit

C,N,W

   

Transition

C,W

Entering State

Entering State

Count All

Units

C,W

 

IP

SI

Value Before Reset

     

Value Per Pulse

C,W

1