Resource File Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Resource File Extensions contain attributes common to Metasys system objects. For details, see Common Object Attributes.

The following table lists the attributes specific to the Resource File extension. Click the attribute name in the table for a description of the attribute. Attributes marked with the letter C are configurable, and attributes marked with the letter W are writable.

Table 1. Resource File Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

File Name

C

 

Category = File

See the File Name section.

Information

C,W

 

Size = 80

Category = Default