Deleting Extensions - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

For a trend extension that is configured to automatically transfer data to a Metasys Server (Repository Enabled = True), be sure to route unforwarded data to the Metasys Server before deleting the trend extension. If you do not, unforwarded trend data is lost.

Procedure

  1. To delete extensions (using the Navigation Tree):
    1. Select the item from the navigation tree and select Show Extensions from the Action menu.
    2. Select the check box of the extension you want to delete.
    3. Click Delete.
  2. To delete extensions (when the item is in the Panel Layout):
    1. View the extension.
    2. Select the tab for the extension.
    3. Select the extension.
    4. Click Delete.