Creating Extensions - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

To create extensions:

Procedure

  1. Select the item from the Navigation Tree and select Show Extensions from the Action menu.
    Note: Alternatively, you can create extensions when prompted upon completion of a wizard, or when the item is in the Panel Layout by selecting the tab for the extension and clicking new.
  2. Select New for the type of extension that you want to create. The corresponding Extension Wizard appears.
  3. Select the attribute that you want to associate with the item.
  4. Complete the information on the wizard screens. The screens vary depending on the type of extension you are creating.
  5. Select Finish on the summary page to create the extension.