Copying and Pasting Extensions - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

Note: You can perform this procedure only in the System Configuration Tool (Offline Mode). You must first create extensions before you can copy and paste them from one item to another. See Creating Extensions for details on how to create extensions.

To copy and paste existing extensions:

Procedure

  1. Select the item from the Navigation Tree that contains the existing extensions that you want to copy, and select Show Extensions from the Action menu. The Extension wizard appears.
    Note: Alternatively, you can right-click the item in the navigation tree and select Show Extensions from the menu that appears.
  2. Select the check box for one or more of the existing extensions that you want to copy.
  3. Click Copy Checked Extensions.
  4. Click Done.
  5. Select the item from the navigation tree that you want to receive the copied extensions, and select Paste from the Edit Menu.
    Note: Alternatively, you can right-click the item in the navigation tree and select Edit > Paste from the menu that appears.

    When you paste an extension, the extension retains the name of the copied extension and appends it with a number.