Averaging Extensions - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Averaging extension calculates the average, minimum, and maximum value of an attribute over a specific interval (for example, space temperature over 24 hours). The extension is able to sample Boolean, Integer, Unsigned, Enumerated, or Float attribute value types for any extendable objects within a BACnet device.

For more information on averaging extensions, see Averaging Attributes.